Diodes Incorporated

观点

Looking Beyond the Datasheet New Ways to Use Devices

超越数据表框架 - 新的方式使用装置

作者:Diodes 公司 Isaac Sibson

 

电流稳流器是一种基本的建构区块,可在任何需要稳定电流来源的电路或装置的地方使用。这些装置也常常在可能产生负面冲击的不稳定电流供应环境中使用。

Read More
Why Logic Makes Sense

我们乐见的正是隐形隐藏逻辑

作者:Diodes 公司 PTC 营销主管 Johnny Lu

 

为什么我们需要逻辑设备

在需要可靠联机甚至克服系统内部设计挑战的情况下,广泛使用的标准逻辑设备,通常是连接电路各部分的首选方式。

Read More
Blog post on smaller packages graphic

麻雀虽小、五脏俱全的小外形封装

作者:Diodes 公司产品营销经理 Shane Timmons

 

轻巧封装的趋势依旧持续

戈登.摩尔 (Gordon Moore) 对集成电路 (IC) 组件密度不断增长的先知灼见仍被证明是正确的。即使近年来这样的成长已经趋缓,但轻巧封装的趋势仍快速持续着。

Read More
Diodes AP3917 image

Efficient Offline Power for Small Online Appliances

By Richard Lin, AC-DC Business Unit Manager

It is widely acknowledged that, at its heart, the Internet of Things (IoT) comprises countless sensors, actuators, and other devices that add ‘intelligence’ to the connected world. For the IoT to work as intended, many of these devices must be switched on and connected 24 hours a day, seven days a week.

Read More
Diodes Incorporateds Synchronous Buck AP6320x

Minimizing EMI in Switched-mode PSUs

By Tu Bui – Senior Marketing/Application Manager

Developers of applications that feature power conversion elements, including home appliances, power tools, industrial and office equipment, will know only too well that electromagnetic interference (EMI) is largely unavoidable. However, they should also know that it can be managed, so that its effects are minimized to the point that they no longer present a problem.

Read More
DIO 6883 AP356xQ MR image

How Hall Effect Switches Enable Autonomous Vehicles

By Charles Kuo, Sensor Marketing Manager

Automotive engineers around the world are immersed in harnessing the latest technologies to bring smart, autonomous vehicles to our roads. Those technologies will also enhance the driver and passenger experience far beyond today’s norm, through intuitive human-machine interfaces and highly personalized cockpits.

Read More
Ultra Low Power Omnipolar Hall Effect Switch DIO 6824 MR Image AH191121

Why Hall Effect Switches Play a Crucial Role in IoT

By Charles Kuo, Worldwide Sensor Marketing Manager

Many words have been written about how the Internet of Things (IoT) will transform the lives of everyone. What is less often said is that at the heart of the IoT is the humble sensor, which enables previously inanimate objects to communicate with each other and to be controlled and monitored.

Read More
High Voltage Buck Converter DIO 6566 PR Image AL17050 MR

如何让无线互联连网物联网装置的功率系统降低待机功耗并提高整合度

作者:Diodes 公司 LED 照明事业部经理 Allan Lin   全世界的家庭和工厂都在拥抱智能技术,通讯与控制系统的连网程度藉由各种无线技术而不断提升,要将便利性与效率带入每个人的生活中。进入物联网 (IoT) 的世界后,我们随时随地都能存取致动器和传感器,用更细腻的角度去检视设备状态,进而将数据传送到云端进行分析,在系统故障之前预先进行维修。例如,我们可以透过 Wi-Fi、Zigbee 或蓝牙低功耗,实时遥控 LED 灯泡,以及选择适合环境的光线色温。 所有这些智能连网装置都需要低待机功耗,这对功率系统设计人员来说是一大挑战。功率转换需在所有负载下维持高效率,包括无线收发器在收发数据封包,或致动器启动时。但是,这些动作其实不常发生,智能系统多数时间都在闲置及等待接收指令,这种「闲置负载」的待机状况对功率转换不佳的系统来说尤其浪费能源。 极大的挑战,便是开发针对各种负载范围将效率优化,拥有恒定稳定输出电压的功率转换器。但由于输出电压会随消耗电流改变,因此这可说是一项相当复杂的设计工作。   法规挑战 对这类系统的开发人员来说,还有除了功率子系统效能以外的更多挑战。全世界有许多不同的法规环境,各个不同国家/地区为了满足其待机功耗、瞬态要求和其他法规,都需要略为不同的功率系统版本。 对智能连网功率系统的开发人员来说,这项设计挑战极为复杂,另外对成本敏感的应用也同样艰难。一个能满足所有要求的设计,其成本可能相当高昂,而且能源效率也可能比针对特定国家/地区优化的装置更低。但若是针对不同地区设计个别的产品与拓扑,要管理所有不同的版本又会产生额外的成本。   高整合度 想要解决这些挑战,我们需要提高智能连网装置功率系统内芯片的整合度。透过在同一封装内整合高电压 MOSFET 开关与功率控制器,不只能满足全球所有的法规要求,还能提供功率效率,并降低待机功耗,花很少的钱就能满足设计人员所需。 例如,AL17050 降压转换器可应用于 85V AC 至 265V AC 的 AC 输入电压范围,无论身处任何地区,皆能安心使用此产品。它可产生 3.…

Read More
Pierce oscillator using CMOS inverter from Diodes Incorporated

晶体振荡器:简易、低成本且高准确度的频率来源

作者:Diodes 公司应用工程部经理 Qin Zhuang   许多电子电路都需要振荡器来同步活动或提供频率参考。 以微控制器为例,频率讯号用于控制数据来往内存的移动、指令的执行,以及外部通讯的速度。另外在无线电系统中,振荡器则提供固定频率,以供发射器与接收器进行通讯。 除了频率,还有一些与振荡器有关的重要属性。像准确度与稳定性 (以百万分之一或 ppm 指定) 对通讯协议和时间记录极为重要。对于便携设备或电池供电的应用来说,低功耗可能是关键的因素。其他需要考虑的特性还有成本,以及频率是否可调。 振荡器会使用某些谐振电路类型的反馈来产生固定频率的输出,谐振电路可作为电阻电容 (RC) 或电感电容 (LC) 网络。这些装置较为简单,且能在宽广的范围内变更频率。但从另一方面来看,这些装置无法提供许多应用所需要的准确度与稳定性。 像是石英等晶体,则因为压电效应,因此可用作谐振器。对晶体施加压力时,晶体内部会产生电压,施加电压时,晶体则会变形。将晶体搭配反馈,便可作为高准确度和稳定性的谐振器,而其自然频率则取决于晶体的大小和裁切方式。     图 1:使用 CMOS 逆变器的皮尔斯振荡器 简单的晶体振荡器 晶体本身是一种被动式组件,需搭配振荡器电路使用。晶体通常整合到需要频率讯号的装置内,例如,微控制器一般会有两个脚位,用来连接晶体和一些外部的负载电容器。这些电容器需与指定的晶体负载电容 (CL) 匹配,确保其能以正确的频率振荡。 变更负载电容器的数值,也会稍微改变振荡频率。我们可以利用电压控制型晶体振荡器 (VCXO) 达到此效果,因为这种振荡器会使用可变电容组件 (变容二极管) 调整频率。 您可用独立型装置来打造外部振荡器,像是使用晶体管或反向逻辑闸极提供放大和反馈。不过,虽然晶体厂商会提供设计指南,但想从头打造出高质量的振荡器却极为复杂。 直接使用现成的振荡器模块,通常会比较方便。振荡器模块包含晶体和振荡器电路,您唯一需要做的,就是为其提供电源。振荡器模块的准确度通常比目标装置内整合的基本电路更为出色。 但尽管晶体非常稳定,但振荡器的频率却可能因供应电压和温度影响而产生变化。要将这些影响降低,可以使用温度补偿晶体振荡器 (TCXO) 模块。TCXO 模块的内部电路可调整频率,藉此补偿温度变化的效应。模块经常也会内含整合式电压稳压器,用于降低外部供应电压变动的效应。TCXO 可达到 2ppm 以上的稳定性。 晶体振荡器提供简易、低成本且高准确度的频率来源,适用于宽广的频率范围,是许多应用类型的合适选择。若要深入了解,请参阅我们关于石英晶体振荡器技术的白皮书,或参阅 Diodes 公司产品页面。      …

Read More
Smallest Secondary Side Synchronous Rectifier Controller for 5V 20V Flyback Power Supplies DIO 6608 PR Image APR346 MR

转向同步整流可以提供脱机电源转换器的效率增益

作者:Diodes 公司产品营销经理吴其昆   您注意到有些东西搭配使用,会产生多么理想的效果吗?我要谈的不是火腿和鸡蛋或盐和胡椒,这些真的只是互补。不,我要谈的是为了真正发挥功效,需要搭配使用的东西,例如凸轮轴与推杆。 把两件东西放在一起,产生一个全新的物品,但仍取决于其组成部分,在自然界相当罕见,然而对于我们这些聪明的工匠来说,这正是我们真正擅长的。在电子业中,这么做非常盛行,更重要的是,在这个领域中,科技可以为我们提供在一致的基础上不断改进的方式。 以电力为例,一般而言总是愈多愈好。我们每获得一项电器产品,就建立了对更多原始电力的需求,因此更有效率地使用电力变得愈来愈重要。这表示在每一个层级,我们都需要更有效率的发电、配电和转换电力的方式。从早期的能源开始,高压交流电一直被视为是有效率的发电和配电方式,当主要产品应用是马达和灯泡时,交流电是很不错的。随着晶体管和集成电路的发明,在局部层级,直流电变得更为重要。 除非我们依据个别情况,开发出可以产生所有所需电力的方式,否则我们仍将继续倚赖高电压交流配电,将电力以管道输送到办公室和家庭。在管道末端会发生转换,从千瓦的交流电降压成毫瓦的直流电。其中的步骤存在效率不彰的问题,电子业正采取措施,以减轻效率低下问题。 这让我们回到了同步性。我们消耗能量的方式,愈来愈多是透过脱机转换,亦即将高压交流电源变成低压直流电源。近期它出现的形式是将电池充电,以供电给便携设备。近期出现的转换拓扑之一,是在二次侧使用一个与一次侧的功率晶体管同步动作的晶体管。次级晶体管取代了效率较差的二极管,也使得此种拓扑结构被命名为:同步整流或 SR。 用行径像二极管的晶体管取代二极管,看起来似乎很没有效率,尤其是通常我们并不认为模仿是一个无损过程。然而在 SR 的情况下,这样做却能提供显著的优点,因为它让关联控制器在可变负载条件下能发挥更大的管理能力。效率的增益百分比取决于 SR 的实作方式,表示我们必须选择正确的解决方案。 以 Diodes 公司生产的次级侧 SR 控制器 APR346 为例。这是一个二次侧 MOSFET 驱动器,支持各种转换器模式,包括连续传导模式、不连续传导模式及准谐振返驰模式,这些模式在脱机转换架构中都很常见。这个装置会感测一次侧 MOSFET 两端的汲极源极电压,并提供正确的闸极驱动器给二次侧 MOSFET。这样一来,它可以在提供 5V 到 20V 直流输出电压的电路中产生更大的效率。这就涵盖了大量的现代产品应用,包括在消费者电子产品中愈来愈重要的 USB 供电 (PD)。   加入像 APR346 这样多用途和能力充足的 SR 控制器,可以在任何脱机转换器中提供秘密源极;由于它省去了使用替代控制器时需要的大量外部组件,还可以降低 BOM…

Read More

1 2 3 4 5 6